Time stamp of /etc/version of distribution image is weird
I follow the instruction of Building the OpenSTLinux distribution to build the distribution image, /etc/version in the image is 20180309123456. Furthermore, the years of most of the directories and files of root filesystem are 2008. If I am correct, it should be the date/time when I built the image.
Why do I ask this? When I tried the built image with the SD card and saw the year of directories and files are 2008, I wondered whether I flashed correct image to the SD card.