U-Boot Developer Build Not Finding libcrypto.so.1.1
Building per the Developer Package Device Tree Building Wiki
Using STM32MP1-Ecosystem_v4.0.0
Verified libssl-dev and libncurses have been installed
openssl version 3.0.0 is present
confirmed libcrypto.so is present at usr/lib/x86_64_linux-gnu
[fiptool] Create fip-stm32mp153a-xpro-mp1-mx-optee.bin fip binary into 'FIP_DEPLOYDIR_FIP' folder...
fiptool: error while loading shared libraries: libcrypto.so.1.1: cannot open shared object file: No such file or directory
[fiptool] Done