U-Boot does not start due to Hash error during USB Boot
We designed original board using STM32MP153D.
We cannot boot by U-boot.
When booting via USB, the Hash check (hash_sha256_check) of the page in the init_runtime of opte_os fails when booting U-Boot (see console log below).
The page that fails is different each time.
SD Card Boot does not fail in Hash check.
What is the cause and what can I do about it?
I/TC: Pager is enabled. Hashes: 2848 bytes
D/TC:0 0 init_runtime:467 Checking hashes of pageable area
D/TC:0 0 init_runtime:473 hash pg_idx 0 hash 0x2ffef4d8 page 0x29800000
D/TC:0 0 init_runtime:473 hash pg_idx 1 hash 0x2ffef4f8 page 0x29801000
D/TC:0 0 init_runtime:473 hash pg_idx 2 hash 0x2ffef518 page 0x29802000
D/TC:0 0 init_runtime:473 hash pg_idx 3 hash 0x2ffef538 page 0x29803000
D/TC:0 0 init_runtime:473 hash pg_idx 4 hash 0x2ffef558 page 0x29804000
E/TC:0 0 init_runtime:476 Hash failed for page 4 at 0x29804000: res 0xffff000f
E/TC:0 0 Panic at core/arch/arm/kernel/boot.c:478 <init_runtime>
E/TC:0 0 assertion 'p->pa' failed at core/arch/arm/mm/core_mmu.c:2433 <io_pa_or_va_secure>
Thank you.