Question
UART4 RX Signal level
I use the UART4 like the following initialization.
void uart4_configuration(void)
{
GPIO_InitTypeDef GPIO_InitStructure;
USART_InitTypeDef USART_InitStructure;
/* enable usart clock */
RCC_APB1PeriphClockCmd(RCC_APB1Periph_UART4, ENABLE);
RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOC, ENABLE);
// Configure USART Tx as alternate function
GPIO_InitStructure.GPIO_OType = GPIO_OType_PP;
GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_UP; //GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL;
GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF;
GPIO_InitStructure.GPIO_Pin = RS485AXM_TX_PIN;
GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz;
GPIO_Init(RS485AXM_COM_PORT, &GPIO_InitStructure);
// Configure USART Rx as alternate function
GPIO_InitStructure.GPIO_OType = GPIO_OType_PP;
GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_DOWN; //GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL;
GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF;
GPIO_InitStructure.GPIO_Pin = RS485AXM_RX_PIN;
GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz;
GPIO_Init(RS485AXM_COM_PORT, &GPIO_InitStructure);
GPIO_PinAFConfig(GPIOC, GPIO_PinSource10, GPIO_AF_UART4);
GPIO_PinAFConfig(GPIOC, GPIO_PinSource11, GPIO_AF_UART4);
USART_StructInit(&USART_InitStructure);
USART_InitStructure.USART_BaudRate = 9600;
USART_Init(UART4, &USART_InitStructure);
USART_Cmd(UART4, ENABLE);
NVIC_EnableIRQ(UART4_IRQn);
}The Rx signal level is abnormal like the following.

The low level is not the zero(ground) level.
But the Tx level is ok like the followings.

Although I detach the RX Pin from the PCB Board, and tie with the TX Pin,
RX/TX Pin level is like the abnormal level(the first image)
Is the initialization is wrong?
Thanks