Unable to connect host PC to STM32MP157C-DK2 Using ST-Link port
I loaded my custom built yocto image into my SD card using the STM32CubeProgrammer and the process was completed successfully.
However, when I toggled the boot switches to boot from SD card, I was not able to connect my host computer (a Ubuntu 20.04 desktop PC) to STM32MP1 board via CN11. When I plugged the micro USB cable from my host computer into CN11 on the STM32MP1 board, my host computer did not detect any new USB device. Can you please advise the steps to troubleshoot this?