Skip to main content
Visitor II
April 16, 2021
Question

Unable to download SDK for stm32mp1

  • April 16, 2021
  • 3 replies
  • 1430 views

Hi,

While following the example at https://wiki.st.com/stm32mpu/wiki/How_to_compile_the_device_tree_with_the_Developer_Package#Updating_the_kernel_device_tree, I'm running into problems downloading the SDK.

The link provided from instructions below, always downloads the "SOURCES" tar not the "SDK".

Developer package:

  • the SDK toolchain, provided within the en.SDK-x86_64-stm32mp1-openstlinux-<YY>-<MM>-<DD>.tar.xz file (download it from st.com)

I have tried searching for the SDK at other places on your web-site, all results bring back the

en.SOURCES-stm32mp1-openstlinux-5-4-dunfell-mp1-20-06-24.tar.xz not the SDK

Could someone please verify this issue and point me to where I can get the SDK.

Thanks in advance!

    This topic has been closed for replies.

    3 replies

    ST Employee
    April 19, 2021

    Hi @JSpra​ ,

    In case you are still stuck with it, you need to click on Yocto_SDK link and not STM32MP1DeveloperPackage.

    Regards,

    Armand

    JSpraAuthor
    Visitor II
    April 19, 2021

    Well, I was running down a device tree compile issue using Yocto SDK, thought I would see if I got same results using STM's suggestion for device tree compile.

    Good suggestion though, thanks for the reply!

    ST Employee
    April 20, 2021

    Hi @JSpra​ ,

    For the device tree compile issue using Yocto SDK I suggest you to create another topic about this, maybe one can help you.

    Armand