unable to upload my code to M4 core in production mode.
Hello,
I have built a custom image using the Yocto project in the Dunfull branch. However, when I try to upload my code to M4 Core in production mode, it shows me this error message. However, I am able to connect to my board through SSH. So I believe it is not a connection issue, and I have tested on the STM32MP157C-DK2 and it does not work either.
I have tested the same procedure on openstlinux Yocto Dunfull, and it worked fine. I am thinking that something is missing in kernel configurations.
I am using Linux version 5.10.116 (oe-user@oe-host) (arm-poky-linux-gnueabi-gcc (GCC) 9.3.0 , GNI ld (GNU biutiles) . 2.34.0.020200910 ) #1 SMP PREEMPT sun May 15 18:00:09 UTC 2022