Uploading flash layout changes with Tf-a 2.6.
Hello,
we (me and @Daniel Laszlo Sitzer ) and are working with a product based on the STM32MP157A and using TF-A, U-Boot (but not OPTEE).
We are in the process for transitioning from TF-A v2.4 to v2.6 and are trying
to understand how we are supposed to transfer the flash layout to TF-A via DFU.
In TF-A v2.4 we used to transfer the flash layout as a STM32 image via DFU to TF-A BL2, then we would transfer a FIP containing another TF-A and U-Boot which would parse the flash layout and expose the correct DFU interfaces to allow for flashing individual partitions.
We noticed that in TF-A v2.6 support for STM32 images was dropped but more importantly support for transferring the flash layout in plat/st/common/stm32cubeprog*_usb.c was removed.
We have understood that by now only FIP is the supported image format for DFU file transfers to TF-A. So we would like to understand if we are supposed to pack the flash layout in to the FIP file that we upload (currently only containing TF-A and U-Boot).