usage of i2c read command in U-Boot
Hi,
I have a custom board with a ST32MP157C and a 24AA025E48 on a i2c bus.
In the U-Boot, I want to read the MAC address located in the 24AA025E48 on the i2c bus 1 at address 0x53 at offset 0xFA.
When I can use the following commands it works (MAC Address: 80:1F:12:36:36:7B)
STM32MP> i2c dev 1
Setting bus to 1
STM32MP> i2c md 53 FA 6
00fa: 80 1f 12 36 36 7b ...66{
STM32MP>
but when i use the i2c read it does not answer anything.
STM32MP> i2c read 53 1 6 FA
STM32MP>
what is wrong with the command ?
who can i do to store the result in a variable in order to change the board ethernet mac address ?
Thanks.