USB ethernet gadget stops working after replugging cable
Not sure if this is the best forum for this question but I am using the USB OTG port in device mode as ethernet gadget. It works fine if plugged in from boot, or first plug in anytime after.
But if unplugged and plugged in again it will not come back without a board reboot:
[ 46.766872] dwc2 49000000.usb-otg: new device is high-speed
[ 46.771014] dwc2 49000000.usb-otg: dwc2_hsotg_enqueue_setup: failed queue (-11)Error -11 is something like "resource temporarily unavailable". Ever seen this before?