USB2514 USB HUB can't connect high-speed devices.
Hi, everybody!
Referring to this topic, I'm still have issue with USB2514 USB HUB:
The description of the problem changed a lot. Currently I'm have two same board with same components and schematic and same images loaded.
One of the board have no problem with USB HUB. All working fine, second board have problem with high speed USB devices:
Here are dmesg's:
keyboard/mouse (full speed):
[ 1449.719724] usb 1-1.1: new full-speed USB device number 11 using ehci-platform
[ 1449.882209] input: Logitech USB Receiver as /devices/platform/soc/5800d000.usbh-ehci/usb1/1-1/1-1.1/1-1.1:1.0/0003:046D:C534.0001/input/input1
[ 1449.961800] hid-generic 0003:046D:C534.0001: input: USB HID v1.11 Keyboard [Logitech USB Receiver] on usb-5800d000.usbh-ehci-1.1/input0
[ 1449.987711] input: Logitech USB Receiver Mouse as /devices/platform/soc/5800d000.usbh-ehci/usb1/1-1/1-1.1/1-1.1:1.1/0003:046D:C534.0002/input/input2
[ 1450.000588] input: Logitech USB Receiver Consumer Control as /devices/platform/soc/5800d000.usbh-ehci/usb1/1-1/1-1.1/1-1.1:1.1/0003:046D:C534.0002/input/input3
[ 1450.090891] input: Logitech USB Receiver System Control as /devices/platform/soc/5800d000.usbh-ehci/usb1/1-1/1-1.1/1-1.1:1.1/0003:046D:C534.0002/input/input4
[ 1450.104322] hid-generic 0003:046D:C534.0002: input: USB HID v1.11 Mouse [Logitech USB Receiver] on usb-5800d000.usbh-ehci-1.1/input1
USB flash:
[ 1451.030141] usb 1-1-port2: Cannot enable. Maybe the USB cable is bad?
[ 1451.940010] usb 1-1-port2: Cannot enable. Maybe the USB cable is bad?
[ 1451.945265] usb 1-1-port2: attempt power cycle
[ 1453.200258] usb 1-1-port2: Cannot enable. Maybe the USB cable is bad?
[ 1454.110142] usb 1-1-port2: Cannot enable. Maybe the USB cable is bad?
[ 1454.115398] usb 1-1-port2: unable to enumerate USB device
Looks, that this HUB can't start in USB HS, but I have no any ideas - why.
For example, another board (same image and DT) :
Flash inserted (high-speed):
[ 25.479763] usb 1-1.2: new high-speed USB device number 3 using ehci-platform
[ 25.645734] usb-storage 1-1.2:1.0: USB Mass Storage device detected
[ 25.671473] scsi host0: usb-storage 1-1.2:1.0
[ 26.240027] usbcore: registered new interface driver uas
[ 26.730883] scsi 0:0:0:0: Direct-Access Kingston DataTraveler II+ PMAP PQ: 0 ANSI: 0 CCS
[ 26.762085] sd 0:0:0:0: Attached scsi generic sg0 type 0
[ 26.887486] sd 0:0:0:0: [sda] 8059904 512-byte logical blocks: (4.13 GB/3.84 GiB)
[ 26.900466] sd 0:0:0:0: [sda] Write Protect is off
[ 26.904557] sd 0:0:0:0: [sda] No Caching mode page found
[ 26.909134] sd 0:0:0:0: [sda] Assuming drive cache: write through
[ 26.995371] sda: sda1
[ 27.021470] sd 0:0:0:0: [sda] Attached SCSI removable disk
Could anybody suggest me which way to debug and what is the most possible reason - SW or HW?...
Thank you in advance
Looking forward for your reply