Use STM32MP157 with 4 lanes DSI display
Hi,
I'm working with the STM32MP157 and I'm trying to interface it with 4 lanes DSI display.
the problem is that the STM32MP157 support only DSI with 2 lanes. In the other hand, I can't program the controller of the display (JD9365DA-H3) to switch with 2 lanes display.
So I want to know if the display can work with only 2 lanes instead of 4.
In general, how we can interface (no programmable) 4 lanes display with STM32MP157
Thank you