Using I2S on stm32mp135f-dk
Hi I am trying to configure I2S with stm32mp135f-dk so that i2s signals are accessible from 40 pin header. I am using the realtime package (build-openstlinuxweston-stm32mp13-rt). I was checking the instruction from you web and it tells that I should enable I2S using menuconfig. I am seeing that I2S is a module that I cannot directly enable. How can I check that this is in the build?
Also I would need some support regarding the device tree configuration. Do I need to run STM32CubeMX and generate new devicetree files to get something activated? Or is there some existing dts file which I could edit and add my i2s driver in use there? It looks like that stm32mp135f-dk.dts does not currently contain any i2s related configuration.