VirtIO problem on STM32MP157C-DK2
Hi! I am working with stm32mp157c-dk2 and trying to establish communication between m4 and a7 cores. I analyze standard examples for this purpose, namely OpenAMP_TTY_echo. VIRT_UART initialization is presented here for m4 core:
log_info("Virtual UART0 OpenAMP-rpmsg channel creation\r\n");
if (VIRT_UART_Init(&huart0) != VIRT_UART_OK) {
log_err("VIRT_UART_Init UART0 failed.\r\n");
Error_Handler();
}
log_info("Virtual UART1 OpenAMP-rpmsg channel creation\r\n");
if (VIRT_UART_Init(&huart1) != VIRT_UART_OK) {
log_err("VIRT_UART_Init UART1 failed.\r\n");
Error_Handler();
}
/*Need to register callback for message reception by channels*/
if(VIRT_UART_RegisterCallback(&huart0, VIRT_UART_RXCPLT_CB_ID, VIRT_UART0_RxCpltCallback) != VIRT_UART_OK)
{
Error_Handler();
}
if(VIRT_UART_RegisterCallback(&huart1, VIRT_UART_RXCPLT_CB_ID, VIRT_UART1_RxCpltCallback) != VIRT_UART_OK)
{
Error_Handler();
}
After flashing is issued:
[ 111.672943] virtio_rpmsg_bus virtio0: creating channel rpmsg-tty-channel addr 0x0
[ 111.678249] virtio_rpmsg_bus virtio0: rpmsg host is online
[ 111.685266] remoteproc0#vdev0buffer: registered virtio0 (type 7)
[ 111.690252] virtio_rpmsg_bus virtio0: creating channel rpmsg-tty-channel addr 0x1
[ 111.696384] remoteproc remoteproc0: remote processor m4 is now up
[ 115.293405] virtio_rpmsg_bus virtio0: creating channel rpmsg-tty-channel addr 0x0
[ 115.299594] virtio_rpmsg_bus virtio0: channel rpmsg-tty-channel:ffffffff:0 already exist
[ 115.307771] virtio_rpmsg_bus virtio0: rpmsg_create_channel failed
[ 115.313773] virtio_rpmsg_bus virtio0: creating channel rpmsg-tty-channel addr 0x1
[ 115.321384] virtio_rpmsg_bus virtio0: channel rpmsg-tty-channel:ffffffff:1 already exist
[ 115.329519] virtio_rpmsg_bus virtio0: rpmsg_create_channel failed
And when viewing tty:
root@stm32mp1:~# ls /dev/tty*
/dev/tty /dev/tty2 /dev/tty31 /dev/tty43 /dev/tty55 /dev/ttySTM0
/dev/tty0 /dev/tty20 /dev/tty32 /dev/tty44 /dev/tty56 /dev/ttyp0
/dev/tty1 /dev/tty21 /dev/tty33 /dev/tty45 /dev/tty57 /dev/ttyp1
/dev/tty10 /dev/tty22 /dev/tty34 /dev/tty46 /dev/tty58 /dev/ttyp2
/dev/tty11 /dev/tty23 /dev/tty35 /dev/tty47 /dev/tty59 /dev/ttyp3
/dev/tty12 /dev/tty24 /dev/tty36 /dev/tty48 /dev/tty6 /dev/ttyp4
/dev/tty13 /dev/tty25 /dev/tty37 /dev/tty49 /dev/tty60 /dev/ttyp5
/dev/tty14 /dev/tty26 /dev/tty38 /dev/tty5 /dev/tty61 /dev/ttyp6
/dev/tty15 /dev/tty27 /dev/tty39 /dev/tty50 /dev/tty62 /dev/ttyp7
/dev/tty16 /dev/tty28 /dev/tty4 /dev/tty51 /dev/tty63
/dev/tty17 /dev/tty29 /dev/tty40 /dev/tty52 /dev/tty7
/dev/tty18 /dev/tty3 /dev/tty41 /dev/tty53 /dev/tty8
/dev/tty19 /dev/tty30 /dev/tty42 /dev/tty54 /dev/tty9
As You can see in /dev/tty* the /dev/ttyRPMSG0 port is not created on the A7 kernel side. Can you please tell me what step I am missing? Thanks in advance!