waveshare display interfacing with stm32mp157c
I have a custom yocto project based on stm32mp157c. I have developed the bootloader and linux kernel.I have display functionalty and display is working perfectly. But now I am changing the display, because the display will be discontinued. The device tree setup for the display is:
&dsi {
#address-cells = <1>;
#size-cells = <0>;
status = "okay";
ports {
#address-cells = <1>;
#size-cells = <0>;
port@0 {
reg = <0>;
dsi_in: endpoint {
remote-endpoint = <<dc_out_dsi>;
};
};
port@1 {
reg = <1>;
dsi_out: endpoint {
remote-endpoint = <&dsi_panel_in>;
};
};
};
panel-dsi@0 {
compatible = "orisetech,otm8009a";
reg = <0>;
rotation = <0>;
address_mode = <0>;
power-supply = <&v3v3>;
status = "okay";
port {
dsi_panel_in: endpoint {
remote-endpoint = <&dsi_out>;
};
};
};
};
This configuration is working perfectly fine. As this display will be discontinued, we decided for waveshare 5 inch display, which is widely used for raspberry pi. But this display compatible parameter is not in the linux kernel. Currently I am using Linux kernel version 5.4.
I have following display:
https://www.waveshare.com/wiki/5inch_DSI_LCD
Can anyone help me to interface display, what should be the compatible parameter and which driver I need to add for this display support. Thanks in advance.