What are the steps needed to use QSPI (QUADSPI) to interface to an FPGA?
Hello!
Board: STM32MP157F using STM32MP15-Ecosystem-v3.1.0
We are using SPI4 to interface and control a FPGA by a custom SPI protocol driver.
This works great!
To get faster data transfer the QSPI interface should be used. The FPGA will deliver data with up to 200MBit/s.
This is how we currently configured SPI4:
/* SPI */
&spi4 {
pinctrl-names = "default", "sleep";
pinctrl-0 = <&spi4_pins_b>;
pinctrl-1 = <&spi4_sleep_pins_b>;
cs-gpios = <&gpioe 11 0>; /* PE11 : SPI4,NSS */
status = "okay";
dspi@0 {
compatible = "dspi4";
reg = <0>; /* CS #0 */
spi-max-frequency = <4500000>;
};
};https://wiki.st.com/stm32mpu/wiki/QUADSPI_device_tree_configuration
only talks about memory and the MTD framework.
Can I use something like this to access QSPI by a custom SPI protocol driver?
This is completely untested and should only serve to show what I want to achieve:
/* QUADSPI */
&qspi {
pinctrl-names = "default", "sleep";
pinctrl-0 = <&qspi_clk_pins_a &qspi_bk1_pins_a &qspi_bk2_pins_a>;
pinctrl-1 = <&qspi_clk_sleep_pins_a &qspi_bk1_sleep_pins_a &qspi_bk2_sleep_pins_a>;
cs-gpios = <&gpiof 6 0>; /* PF6 : GPIO8,SPI5,NSS */
status = "okay";
dqspi@0 {
compatible = "dqspi";
reg = <0>; /* CS #0 */
spi-max-frequency = <15000000>;
};
};Is it possible to access QSPI by using spidev driver and tools?
Thank you for your help!
Bye Gunther