What is the maximum transmission interprocessor bandwidth on STM32MP1?
I am interested in the maximum transmission bandwidth between the A7 core and M4 core on the STM32MP1.
I did some test using RPMsg framewirk and sent messages with length 496 Byte from the A7 core to the M4 core. Therefore I modified the OpenAMP_raw example. I measured the time which it takes to receive 2300 messages on the M4 side using HAL_getTick(). I measured an average time of 132 ms, which would result in a transmission bandwidth of just 8,64 MB/s, which seems pretty slow to me.
Has anyone made some experience with it or did some similar evaluation? Maybe me measurement method isnt optimal? I am thankful for evey opinion.