Skip to main content
Graduate
June 2, 2022
Question

What is the schematics for STM32MP157 to use just the ADC

  • June 2, 2022
  • 2 replies
  • 1141 views

Hello every one I am starting with the STM32MP157, and i wonder if there is a schematis that i can follow that doesn't require the use of external DRAM or any IC meaning without (linux) using bare meatal code through the IDE. just to operate the ADC ?

in this case i please seek your help for experts or any one that has a clue on STM32MP1s.

thank you

    This topic has been closed for replies.

    2 replies

    Technical Moderator
    June 3, 2022

    Hi @iheb​ ,

    Could you please precise rationale to use STM32MP1 Series without using Linux nor DRAM ?

    Note that Cortex-A bare-metal is not supported by ST deliveries, you should do it by yourself or use 3rd party products (e.g. ST partners).

    Maybe worth to look at using STM32H7 Series which provide very similar ADC features as well as dual processor.

    Regards.

    Graduate II
    June 3, 2022

    #JamaicanUpHillBobsledTeam

    Graduate II
    June 3, 2022

    If you plan to bare-metal these chips you're going to need to be a lot more resourceful and self-reliant, or hire staff that can work on them despite the documentation, or direction of the tide.