Skip to main content
Graduate II
May 2, 2024
Solved

Which manufacturer can produce the example CAD reference?

  • May 2, 2024
  • 1 reply
  • 1063 views

I have build a board of STM32MP151AAC3 processor. It has almost everything, except audio output and DSI Display. STM32MP151 series does not support DSI.

Anyway! I used the included Design Rules from that CAD file  .

The Design Rules are narrow and tight, so not even JLCPCB can produce this board. 

Question:

Which manufacturer can produce this board if the design rules looks like this?

This is an open source project, so I will upload this on GitHub later.

Skärmbild 2024-05-03 000819.pngSkärmbild 2024-05-03 000838.png

 

Skärmbild 2024-05-03 000448.pngSkärmbild 2024-05-03 000429.pngSkärmbild 2024-05-03 000401.png

    This topic has been closed for replies.
    Best answer by DMårt

    @GCici 

    Thank you. I found out that JLCPCB can produce this board. They approved my design even if I have a minimum clearance of 0.08mm.

    1 reply

    Visitor II
    May 10, 2024

    Hi,

    even though this isn't the most suitable place to ask, you can try Hi-Tech corp if you need EU production.

    Cheers

    DMårtAuthorAnswer
    Graduate II
    May 11, 2024

    @GCici 

    Thank you. I found out that JLCPCB can produce this board. They approved my design even if I have a minimum clearance of 0.08mm.