Skip to main content
Visitor II
July 11, 2021
Solved

Why kernel name does not change after sync & reboot commands?

  • July 11, 2021
  • 3 replies
  • 1391 views

Good evening,

I am using stm32mp157F-DK-2 board. And I want to update the kernel from old 5.4.31 to 5.10.10.

I was following step-by-step "Modify, rebuild and reload the Linux® kernel" on the "https://wiki.st.com/stm32mpu/wiki/Getting_started/STM32MP1_boards/STM32MP157x-DK2/Develop_on_Arm%C2%AE_Cortex%C2%AE-A7/Modify,_rebuild_and_reload_the_Linux%C2%AE_kernel#Build_the_Linux-C2-AE_kernel_source_code_for_the_first_time".

Only strange thing the command: >> /sbin/depmod -a - does not return any success/failure info. No errors appeared so I used >> sync and >>reboot.

After reboot I see that both old and new kernel modules are present:

>> ls /lib/modules

5.10.10  5.4.31

When i try to check current kernel version :

>> uname -a

Linux stm32mp1 5.4.31 #1 SMP PREEMPT Wed Apr 8 07:08:47 UTC 2020 armv7l armv7l armv7l GNU/Linux

Have I missed something? Does the old kernel module should be removed entirely?

I have tried re-flashing the board and repeating procedure multiple times. Thanks for any information!

    This topic has been closed for replies.
    Best answer by OlivierK

    Hi ACELK.1 (Community Member)

    You shouldn't have 5.4.x modules mixed with 5.10.x. I suggest that you start from a clean directory, different from your old kernel 5.4 environment.

    Install the Developper package (OpenSTLinux V3.x) following the link you mentioned, and source the SDK environment (V3.x) before you rebuild the kernel:

    source <STM32MPU-Release-21-03-31 Dev Package Dir>/SDK/environment-setup-cortexa7t2hf-neon-vfpv4-ostl-linux-gnueabi

    The boot partitions should be updated also according to OpenSTLInux V3.x. If not done so, you can flash a OpenSTLinux V3,x starter package then update the kernel according to your needs.

    Best Regards

    Olivier

    3 replies

    OlivierKAnswer
    Technical Moderator
    July 12, 2021

    Hi ACELK.1 (Community Member)

    You shouldn't have 5.4.x modules mixed with 5.10.x. I suggest that you start from a clean directory, different from your old kernel 5.4 environment.

    Install the Developper package (OpenSTLinux V3.x) following the link you mentioned, and source the SDK environment (V3.x) before you rebuild the kernel:

    source <STM32MPU-Release-21-03-31 Dev Package Dir>/SDK/environment-setup-cortexa7t2hf-neon-vfpv4-ostl-linux-gnueabi

    The boot partitions should be updated also according to OpenSTLInux V3.x. If not done so, you can flash a OpenSTLinux V3,x starter package then update the kernel according to your needs.

    Best Regards

    Olivier

    Visitor II
    July 12, 2021

    Thank, Olivier,

    I am trying cleaning all directories and re-doing everything from scratch. Just couple of questions poped-up - if you don't mind.

    1.The boot partitions should be just copied from my 5.10.10 work directory, or do I have to update the Bootfs according to?

    7.2. Update via network:

    ------------------------

    * kernel + devicetree

      $ cd <path to install_artifact dir>/install_artifact

      if bootfs are not monted on target, mount it

        $ ssh root@<ip of board> df to see if there is a partition mounted on /boot

      else

        $ ssh root@<ip of board> mount <device corresponding to bootfs> /boot

      $ scp -r boot/* root@<ip of board>:/boot/

      $ ssh root@<ip of board> umount /boot

    or just these two copy commands are enough ?

    scp arch/arm/boot/uImage root@<board ip address>:/boot

    scp arch/arm/boot/dts/stm32mp157*.dtb root@<board ip address>:/boot

    2.So just to clarify after successful kernel update & sync & reboot, the BOARDs /lib/modules should only contain the latest module's name?

     Best Regards, Arnas, LCC Simbiotecha

    Visitor II
    July 13, 2021

    UPDATE: I have cleaned the directory and refollowing the steps in "Modify, rebuild and reload the Linux® kernel", but kep having issues -like boot getting stuck or version not changing after reboot.

    So in the end I have followed Oliver's advice, re'flashed the board via USB-C by using the 5.10.10 flash image on the en.FLASH-stm32mp1-openstlinux-5.10-dunfell-mp1-21-03-31.tar.xz, from : https://wiki.st.com/stm32mpu/wiki/STM32MP1_Starter_Package_-_images. Everything seems to be working fine now, thanks!

    Visitor II
    July 13, 2021

    But it is still unclear, why i could not do that successfully after cleaning the directory.... Is there a chance to perhaps get a video tutorials, of step-by-step for kernel-configuration-uploading ?