why M4 firmware been stopped by linux side access uart8@40019000 on STM32MP157C need confirmation of stm32-rproc would stop M4 firmware loaded by u-boot need confirmation on stm32-rproc has issue with kernel 5.10.10
After linux bootup on STM32MP157C custom board with kernel build 5.4.31, I load and start M4 with remoteproc successfully, but every time when linux access uart8@40019000, M4 side firmware stopped, the two command i used to test is "echo 123 > /dev/ttySTM1" or "stty -F /dev/ttySTM1 -a", both command stopped the M4 firmware, and my M4 firmware is toggling a GPIO when it's running, so it's been confirmed by using logic analyzer.
Would anyone can tell me what's going on, and device tree dts file has been attached.
Another thing I observed is, if I load M4 firmware by u-boot, during linux side boot up, M4 firmware been stopped by some driver, I suspecting it's stopped when remoteproc driver been probed.
With kernel 5.10.10, the stm32-rproc driver failed to reset M4 and probe M4. would someone can confirm it?