Skip to main content
Visitor II
August 2, 2019
Question

why the system workbench use stklink?

  • August 2, 2019
  • 1 reply
  • 819 views

Hi, I use system workbench to debug example project. The serial port and ethernet over usb are recognized by system workbench. Now, the debuger step is using openocd to connect target board. I follow the below link to setting the debug configuration options.

https://wiki.st.com/stm32mpu/wiki/Getting_started/STM32MP1_boards/STM32MP157C-DK2/Develop_on_Arm%C2%AE_Cortex%C2%AE-M4/Modify,_rebuild_and_reload_a_firmware

0690X0000097zpKQAQ.png

    This topic has been closed for replies.

    1 reply

    Visitor II
    August 4, 2019

    0690X000009813hQAA.pngIt uses OpenOCD (STLink) by default. Did you correctly set "thru Linux Core" in Startup tab, shown in the picture?

    SChen.11Author
    Visitor II
    August 4, 2019

    I had select the production mode on startup tab window.Below is the screenshot.

    0690X000009814QQAQ.png

    SChen.11Author
    Visitor II
    August 4, 2019

    I use reinstall ubuntu 14.04 64bit to test it. It's also failed and got another error.

    0690X0000098170QAA.png