Skip to main content
Graduate II
June 8, 2025
Question

Will DSI -> HDMI show the boot screen at startup?

  • June 8, 2025
  • 1 reply
  • 420 views

The DSI can be transformed to HDMI using the ADV7535BCBZ chip. 

My question is: Will I be able to see the boot screen at startup directly when the HDMI is plugged in and Linux is booting? Or must Linux start the DSI later after the booting process?

This is for the STM32MP257FAK. 

    This topic has been closed for replies.

    1 reply

    ST Employee
    June 18, 2025

    Hi,

    if HDMI is plugged at startup, there will be no "ST" splash screen during uboot.

    Philippe.