Skip to main content
Visitor II
February 28, 2019
Solved

Witch STM32 chip for my project ?

  • February 28, 2019
  • 2 replies
  • 1877 views

Hi everybody!

I working on a simple project but with some sensors and co.

I'm newbie with the STM32 and I want to try to port the project from the ATmega2560 to the STM32.

But witch chip?

I need :

> SPI for an TFT screen 2.2" (ILI9340C or ILI9341)

> SPI for a MicroSD Card

> BMP180 sensor

> 2 pins interup

> 3 indepedants Pins PWM

> 2 ADC

> RTC time

> One Serial for bluetooth HC-05

> One Serial for an GPS L80

> One Serial for connect an external probe

> 10 digital Input

> 4 digital Output

> min 72Mhz for the sreen

> All pin in 3.3v

Question :

> Minimum 64K of program space ?

> Flashing the MPU directly with the USB port ?

> Possible to program all from the Arduino IDE ? ( with the right card )

Thanks! =)

    This topic has been closed for replies.
    Best answer by Uwe Bonnes

    Play with the MCU selector.

    2 replies

    Graduate II
    February 28, 2019

    Play with the MCU selector.

    Visitor II
    March 22, 2019

    The cheap STM32F103 should manage that. Google for Blue Pill as a suitable test bed.