Skip to main content
Visitor II
May 18, 2021
Solved

X-NUCLEO-PLC01A1 Compatibility with STM32MP157-DK2

  • May 18, 2021
  • 1 reply
  • 810 views

I'm connecting a X-NUCLEO-PLC01A1 with my DK2 card. The Inputs are working fine and for the outputs I can read the fault status , I'm getting 0000 0000 1000 0101, then all is right, the 3 error leds are off, and the OE signal is in 0 (I tested also with OE = 1); but I not getting anything in the outputs.

I can see in the diagram that one of the leds is named PG (Power good) but it's off. I connected the GND / 24V to the left of the input connector. The led turns flash when I power on/off the system.

Then I have two problems, the PG led and the outputs.

I appreciate any insights

Thanks

    This topic has been closed for replies.
    Best answer by HSant.1

    Hi, I solved all my problems, the PG signal is active in 1 , like we can see in the X-NUCLEO-PLC01A1 , in the datasheet the explanation is ok, but they put the inverted signal over the PG, don't know why. The outputs were in 0 because of the watchdog, once I begin to toggle CS1 signals it works.

    1 reply

    HSant.1AuthorAnswer
    Visitor II
    May 25, 2021

    Hi, I solved all my problems, the PG signal is active in 1 , like we can see in the X-NUCLEO-PLC01A1 , in the datasheet the explanation is ok, but they put the inverted signal over the PG, don't know why. The outputs were in 0 because of the watchdog, once I begin to toggle CS1 signals it works.