Skip to main content
Explorer
July 10, 2024
Question

X-STM32MP-GNSS2 board - Linux

  • July 10, 2024
  • 1 reply
  • 829 views

Hello, I have the STM32MP157-DK2 board and the GNSS2 eval board (w/Taoglas antenna) and I am trying to follow UM2909 (getting started).  It seems the ST Wiki is updated past the UM2909.  For example  in 3.3 titled “Downloading the kernel sources (developer package)” the link the kernel sources (titled “Modify, rebuild and reload the Linux kernel” goes to a wiki page that is labeled NRND.  If I start the wiki from scratch, I go to a different wiki page:

 

https://wiki.st.com/stm32mpu/wiki/STM32MP157x-DKx_-_software_distributions

 

The instructions on this page (going to the Yocto build) are not complete or they are different.

 

Any help/suggestions are appreciated. If it makes sense to follow the NRND pages, I can do that - but my Linux is not as strong as I would like.  I am willing to start from scratch if necessary as well but if there are any insights out there I do appreciate the help.  Thank you.

    This topic has been closed for replies.

    1 reply

    ST Employee
    July 22, 2024

    Hello @rick2399 , 

    You can follow this link to download the kernel and SDK : Modify, rebuild and reload the Linux® kernel - stm32mpu

    or directly from www.st.com : STM32MP1Dev - STM32MP1 OpenSTLinux Developer Package - STMicroelectronics 

    Kernel sources are here : en.SOURCES-stm32mp1-openstlinux-6.1-yocto-mickledore-mpu-v24.06.26.tar\stm32mp1-openstlinux-6.1-yocto-mickledore-mpu-v24.06.26\sources\arm-ostl-linux-gnueabi\linux-stm32mp-6.1.82-stm32mp-r2-r0

     

    Thanks,

    S