Cube IDE debug doesn't work on stm32mp157a-DK1
Hi,
I'm having an issue while trying to debug the OpenAMP_TTY_ECHO_CM4 example described in gettin' started guide for stm32mp157a-DK1 (here link) using Cude IDE 1.4.2 on windows 10 machine. I configure the debug session as describe in the guide section 7, but when I started it, I got the following messages:
Open On-Chip Debugger 0.10.0+dev-g30d1303 (2020-06-18-09:13)
Licensed under GNU GPL v2
For bug reports, read
http://openocd.org/doc/doxygen/bugs.html
srst_only srst_pulls_trst srst_gates_jtag srst_open_drain connect_deassert_srst
Info : Listening on port 6666 for tcl connections
Info : Listening on port 4444 for telnet connections
Info : STLINK V2J37M26 (API v2) VID:PID 0483:3752
Info : Target voltage: 3.220093
Info : Unable to match requested speed 8000 kHz, using 4000 kHz
Info : Unable to match requested speed 8000 kHz, using 4000 kHz
Info : clock speed 4000 kHz
Info : stlink_dap_op_connect(connect)
Info : SWD DPIDR 0x6ba02477
Info : stlink_dap_op_connect(connect)
Info : SWD DPIDR 0x6ba02477
Info : STM32MP157CAAx.cm4: hardware has 6 breakpoints, 4 watchpoints
Info : STM32MP157CAAx.cpu0: hardware has 6 breakpoints, 4 watchpoints
Info : STM32MP157CAAx.cpu1: hardware has 6 breakpoints, 4 watchpoints
Info : STM32MP157CAAx.cm4: external reset detected
Info : starting gdb server for STM32MP157CAAx.cpu0 on 3334
Info : Listening on port 3334 for gdb connections
Info : starting gdb server for STM32MP157CAAx.cm4 on 3333
Info : Listening on port 3333 for gdb connections
Info : accepting 'gdb' connection on tcp/3333
Info : Halt timed out, wake up GDB.
Error: timed out while waiting for target halted
Error executing event gdb-attach on target STM32MP157CAAx.cm4:
Info : New GDB Connection: 1, Target STM32MP157CAAx.cm4, state: reset
Warn : negative reply, retrying
Warn : negative reply, retrying
Warn : target not halted
Info : target STM32MP157CAAx.cm4 was not halted when resume was requested
When I reopen a serial console on cube IDE to run the test (according to guide section 8), I can't find any /dev/ttyRPMSG0 or /dev/ttyRPMSG1 device.
Please someone could help?
Marco.