CubeIDE v1.4.0 is not stopping on breakpoint
I'm trying to make FreeRTOS application which is involving ADC and sending messages via virtual UART to Cortex A7. So I began with example called OpenAMP_FreeRTOS_echo in the cube fw version 1.2.0. That example worked good. I saw echo on /dev/ttyRPMSG0. Then I tried to incorporate ADC into that code but without success (I made succes with ADC + virtual UART without using FreeRTOS, but I want to make FreeRTOS working). I had a lot of trouble using System Workbench in terms of ST-Link detection (I always had to change COM port in the Debug Configuration) and I read on this forum that there were troubles in using FreeRTOS and those troubles are solved in Cube IDE 1.2.1.
https://community.st.com/s/question/0D50X0000BI0vctSQB/freertos-does-not-run-on-stm32mp1-m4-core
So I recently switched to Cube IDE v1.4.0, but there I have trouble on stopping on breakpoint. I placed break point on lines after main which must be executed (i.e. HAL_Init), but the debug is not stopped.
Thanks in advance for the answer,
Nenad