CubeMX 6.10~6.12.1 can not generate stm32mp157 M4 qspi code
Cubeide 1.13 and CubeMX 6.9 can generate the valid code for stm32mp157,but Cubeide 1.14 and CubeMX 6.10 can not! is there a bug or the CubeMX 6.10 have some change for stm32mp157?. MCU Package 1.6.0 and the STMH7xx doesn`t affect it.
void MX_QUADSPI_Init(void)
{
/* USER CODE BEGIN QUADSPI_Init 0 */
/* USER CODE END QUADSPI_Init 0 */
/* USER CODE BEGIN QUADSPI_Init 1 */
/* USER CODE END QUADSPI_Init 1 */
/* USER CODE BEGIN QUADSPI_Init 2 */
/* USER CODE END QUADSPI_Init 2 */
}
why?