Associate II
October 7, 2019
Question
CubeMX (linux OS) Version 5.3.0 generates a devicetree file which is not compiling.
- October 7, 2019
- 3 replies
- 1226 views
I upgraded CubeMX (linux OS) to Version 5.3.0 and the devicetree file is not compiling anymore.
I'm attaching the ioc File and the dts for reference.
it seems some properties (automatically generated) have the string "sleep_sleep" appended which seems wrong to me - I corrected these properties (by editing the dts file) - I got it to compile successfully but the kernel doesn't start now.
This process was working fine with an older CubeMX.
Aurelian