Skip to main content
aman.32
Associate II
July 30, 2019
Solved

Does the STM32CubeIDE 1.0.2 ( windows 10) support STM32MP157?

  • July 30, 2019
  • 4 replies
  • 2178 views

..

This topic has been closed for replies.
Best answer by Olivier GALLIEN

Hi @aman.32​ 

Yes STM32CubeIDE V1.1.0 supporting MP1 is about to be available on st.com along with the new V1.1.0 STM32MP15 ecosystem release.

Refer to Release note and stay tune

https://wiki.st.com/stm32mpu/index.php/STM32MP15_ecosystem_release_note

Olivier

4 replies

victor.b
Associate II
August 1, 2019

Not yet, I belive it will soon support it.

In the meanwhile there is the famous and broken SW4STM32 or there is Keil, witch i switched to and it works flawlessly.

aman.32
aman.32Author
Associate II
August 2, 2019

Thank you. My current Keil uVision is 5.24.2. Do I need to update the software?

PFran.17
Associate
October 14, 2019

Hi,

in October 2019 is not still supported. Is there any update scheduled soon?

Olivier GALLIEN
Olivier GALLIENBest answer
Technical Moderator
October 15, 2019

Hi @aman.32​ 

Yes STM32CubeIDE V1.1.0 supporting MP1 is about to be available on st.com along with the new V1.1.0 STM32MP15 ecosystem release.

Refer to Release note and stay tune

https://wiki.st.com/stm32mpu/index.php/STM32MP15_ecosystem_release_note

Olivier

Olivier GALLIEN In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.