Failed to firmware upgrade ST-LINK firmware on STM32MP157F-DK2 board using STM32CubeProgrammer version 2.12
Hi,
I am using STM32CubeProgrammer version 2.12 running on Windows 10 to connect to the STM32MP157F-DK2 board ST-LINK connector CN-11.
I managed to connect and when I click "Firmware upgrade" the STLinkUpgrade 3.4.0 window opens.
However, when I press "Open in update mode" I get the error message:
Error connecting to device ST-LINK/V2-1 (error 0x3); check USB connection and refresh the device list
At this point the connection is dropped and I have to connect again.
I also noticed that the "Current Firmware" was not listed as I expected from my experience of upgrading the ST-LINK firmware on other NUCLEO and DISCOVERY boards.
Maybe the current version of STM32CubeProgrammer doesn't yet support the STM32MP157F-DK2 board ?
Any help would be much appreciated.
Kind regards,
Steinar