Hi, I am following the Wiki to get started with a STM32MP157C-DK2 but trying to flash I get a segmentation fault error. Error below. I am using a generic micro SD card, as the one supposed to be with the kit was not there. How can I solve this?
alex@NUC:~/Projects/stm32mp1/ecosystem/starter-package/stm32mp1-openstlinux-4.19-thud-mp1-19-10-09/images/stm32mp1$ STM32_Programmer_CLI -l usb -------------------------------------------------------------------
STM32CubeProgrammer v2.2.1
-------------------------------------------------------------------
===== DFU Interface =====
Total number of available STM32 device in DFU mode: 1
Device Index : USB1
USB Bus Number : 001
USB Address Number : 002
Product ID : DFU in HS Mode @Device ID /0x500, @Revision ID /0x0000
Serial number : 002900373338510534383330
Firmware version : 0x0110
Device ID : 0x0500