Skip to main content
Subhajit.Ghosh
Associate
February 27, 2021
Solved

How to change the CPU clock frequency on STM32MP157F-EV1 board from 650MHz to 800MHz?

  • February 27, 2021
  • 2 replies
  • 1862 views

I noticed that even if I create a new project using STM32CubeMX IDE for STM32MP157F-EV1 board, in the clock configuration, the MPUSS_CK is 650MHz. In Linux, I can see the CPU frequency is 650MHz only. How can I clock the CPU to 800MHz as supported by the SoC?

This topic has been closed for replies.
Best answer by Olivier GALLIEN

Hi @Subhajit.Ghosh​ ,

Which version of CubeMX and OpenSTLinux are you using ?

STM32MP157F-EV1 require at least OSTL Openstlinux-5.4-dunfell-mp1-20-06-24  and CubeMX V6.0

Did you test with the default Starter Package provided ?

If not already done you can refer to :

https://wiki.st.com/stm32mpu/wiki/How_to_change_the_CPU_frequency

Olivier

2 replies

Olivier GALLIEN
Olivier GALLIENBest answer
Technical Moderator
March 8, 2021

Hi @Subhajit.Ghosh​ ,

Which version of CubeMX and OpenSTLinux are you using ?

STM32MP157F-EV1 require at least OSTL Openstlinux-5.4-dunfell-mp1-20-06-24  and CubeMX V6.0

Did you test with the default Starter Package provided ?

If not already done you can refer to :

https://wiki.st.com/stm32mpu/wiki/How_to_change_the_CPU_frequency

Olivier

Olivier GALLIEN In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
Subhajit.Ghosh
Associate
March 23, 2021

Hi Olivier,

Apologies for replying late. Thanks for the link.

Did a little bit of digging and found the same link which you have shared and managed to fix the issue.

Yes, we are using the Dunfell release.

The issue was:

We started initial development using the stm32mp157c variant which supports 650MHz.

We were using the device tree source file for tf-a spitted out CubeMX for the "c" variant

in which "stm32mp15xc.dtsi" was included, now the OPP table in this only contains definitions for 650MHz.

After inclusion of "stm32mp15xf.dtsi" for tf-a, there are two operating points now - 400MHz and 800MHz

as per the well written article in the link.

For testing did the following from userspace:

## This shows the current frequency in KHz, below output shows that the CPU is running in 400MHz ##

# cat /sys/devices/system/cpu/cpufreq/policy0/scaling_cur_freq

400000

## This shows the CPU frequency scaling policies available in the linux kernel

# cat /sys/devices/system/cpu/cpufreq/policy0/scaling_available_governors

conservative userspace powersave ondemand performance schedutil 

## This shows which policy is currently active.

# cat /sys/devices/system/cpu/cpufreq/policy0/scaling_governor

ondemand

## This changes the policy to "userspace", so that user can manually input the frequency.

# echo userspace > /sys/devices/system/cpu/cpufreq/policy0/scaling_governor

## Now we can manually change the frequency to 800MHz.

# echo 800000 > /sys/devices/system/cpu/cpufreq/policy0/scaling_setspeed 

## This shows that the current CPU frequency is switched to 800MHz.

# cat /sys/devices/system/cpu/cpufreq/policy0/scaling_cur_freq

800000

Regards,

Subhajit Ghosh