How to generate stm32mp157c-dk2.dts with stm32cubeide?
Hi,
I used the STM32CubeIde version 1.4.
Below is the procedure create "stm32mp157c-dk2.dts ":
1) onpen STM32CubeIde
2) Click "File->New->STM32 Project" to create a project "stm32mp157c-dk2"
3)Click "Board Selector" to select board "STM32MP157C-DK2"
4)Configure project name "stm32mp157c-dk2"
5) press "Yes" to "initialize all peripherals with their default Mode"
6)Click "Project->Generate Code" to generate code.
The generated device tree file is different from device tree file in "en.SOURCES-stm32mp1-openstlinux-5-4-dunfell-mp1-20-06-24.tar.xz".
Please advise how i can get the same device tree file.
Can you share me with the "*.ioc" file which generated device tree file in the "en.SOURCES-stm32mp1-openstlinux-5-4-dunfell-mp1-20-06-24.tar.xz".
Thanks,
QiZhang
I