Good afternoon.I tried to create a demo project (STM32MP157C-DK2\Demonstrations\Al_Character_Recognition) for the STM32MP157D_DK1 board. When assembling, I had a problem.(Gluk_test_1) How to include the library in the project correctly? Sincerely, Alexander.
"To give better visibility on the answered topics, please click on ""Accept as Solution"" on the reply which solved your issue or answered your question."
Please close this post by clicking the "Select as Best" button in the above answer. This will help other community members to find the solution more quickly.
Thank you.
"To give better visibility on the answered topics, please click on ""Accept as Solution"" on the reply which solved your issue or answered your question."
Good afternoon. Thanks for the help. But, unfortunately, the problems remained. I really need an example of working on STM32MP157D-DK RTC and working with a graphical application. I tried to make an example of using RTC myself. But, unfortunately, it works once. I used python 3. Where did I go wrong? Sincerely, Alexander.
Did you succeed to link the library? you said "But, unfortunately, it works once", so I think yes.. and you have another issue ..
SofLit
"To give better visibility on the answered topics, please click on ""Accept as Solution"" on the reply which solved your issue or answered your question."
Good afternoon, I have written two versions of the time output test programs to the console for STM32MP157D. Both programs work no more than 2 hours, then the system restarts. What did I do wrong?
I think the original question was answered (How to include the library in the project correctly?) and this is a new issue.
Could you please open a new thread for this new issue?
Thank you ..
"To give better visibility on the answered topics, please click on ""Accept as Solution"" on the reply which solved your issue or answered your question."
No. I got around this problem. The problem with the unstable operation of the STM32MP157D-DK board. The operation of the time output program on the console leads to a restart of the system after an hour (Openstlinux)
For the efficiency and to have answers from the community members, It's better for you to open another thread with the right title.. Otherwise, I'm afraid, you have a risk to not get an answer ..
"To give better visibility on the answered topics, please click on ""Accept as Solution"" on the reply which solved your issue or answered your question."