I am not able to burn partitions using STMProgramer and i am not able to read or using the SD card
hello
I am using a STM32M15 into a custom board
i am trying to use STMBoard to burn my system
this is the .tsv that i am using
#Opt Id Name Type IP Offset Binary
- 0x01 fsbl1-boot Binary none 0x0 tf-a-stm32mp157c-ya157c-512d-v2-serialboot.stm32
- 0x03 ssbl-boot Binary none 0x0 u-boot-stm32mp157c-ya157c-512d-v2-trusted.stm32
P 0x04 fsbl1 Binary mmc1 boot1 tf-a-stm32mp157c-ya157c-512d-v2-trusted.stm32
P 0x05 fsbl2 Binary mmc1 boot2 tf-a-stm32mp157c-ya157c-512d-v2-trusted.stm32
P 0x06 ssbl Binary mmc1 0x00084400 u-boot-stm32mp157c-ya157c-512d-v2-trusted.stm32
P 0x07 debian System mmc1 0x00384400 fl4-debian-10.ext4
all files are in the same folder
$ ls -l
total 692364
-rw-r--r-- 1 som som 521 Jul 20 14:42 fl4-debian-10-emmc.tsv
-rw-rw-rw- 1 root root 1073741824 Jul 20 12:18 fl4-debian-10.ext4
-rw-r--r-- 1 som som 860 Jul 20 14:51 FlashLayout_emmc_stm32mp157c-ya157c-512d-v2-trusted.tsv
-rw-r--r-- 1 som som 241984 Jul 20 13:36 tf-a-stm32mp157c-ya157c-512d-v2-serialboot.stm32
-rw-r--r-- 1 som som 241984 Jul 20 13:36 tf-a-stm32mp157c-ya157c-512d-v2-trusted.stm32
-rw-r--r-- 1 som som 874729 Jul 20 13:37 u-boot-stm32mp157c-ya157c-512d-v2-trusted.stm32
the error is:
-------------------------------------------------------------------
STM32CubeProgrammer v2.7.0
-------------------------------------------------------------------
Serial Port /dev/ttyUSB0 is successfully opened.
Port configuration: parity = even, baudrate = 115200, data-bit = 8,
stop-bit = 1.0, flow-control = off
Activating device: OK
Chip ID: 0x500
BootLoader protocol version: 4.0
Device name : STM32MP1
Device type : MPU
Device CPU : Cortex-A7
Start Embedded Flashing service
Error: TSV file erasing-board.tsv not conform: it may miss some columns or fields
Error: TSV flashing service failed
Then i try to burn a default image from STM resourses:
:~/Downloads/MYD-YA157C-20210520/02_Images/myir-image-full$ STM32_Programmer_CLI -c port=/dev/ttyUSB0 -w flashlayout_myir-image-full/trusted/erase.tsv
-------------------------------------------------------------------
STM32CubeProgrammer v2.7.0
-------------------------------------------------------------------
Serial Port /dev/ttyUSB0 is successfully opened.
Port configuration: parity = even, baudrate = 115200, data-bit = 8,
stop-bit = 1.0, flow-control = off
Activating device: OK
Chip ID: 0x500
BootLoader protocol version: 4.0
Device name : STM32MP1
Device type : MPU
Device CPU : Cortex-A7
Start Embedded Flashing service
Memory Programming ...
Opening and parsing file: tf-a-stm32mp157c-ya157c-512d-v2-serialboot.stm32
File : tf-a-stm32mp157c-ya157c-512d-v2-serialboot.stm32
Size : 241984 Bytes
Partition ID : 0x01
Download in Progress:
[==================================================] 100%
File download complete
Time elapsed during download operation: 00:00:28.396
RUNNING Program ...
PartID: :0x01
Start operation done successfully at partition 0x01
GETPHASE command not acknowledged!
Reemission of GetPhase command
Flashlayout Programming ...
[==================================================] 100%
Running Flashlayout Partition ...
Flashlayout partition started successfully
Memory Programming ...
Opening and parsing file: u-boot-stm32mp157c-ya157c-512d-v2-trusted.stm32
File : u-boot-stm32mp157c-ya157c-512d-v2-trusted.stm32
Size : 874729 Bytes
Partition ID : 0x03
Download in Progress:
[==================================================] 100%
File download complete
Time elapsed during download operation: 00:01:42.503
RUNNING Program ...
PartID: :0x03
Start operation done successfully at partition 0x03
GETPHASE command not acknowledged!
Reemission of GetPhase command
GETPHASE command not acknowledged!
Reemission of GetPhase command
GETPHASE command not acknowledged!
Error: GetPhase command not acknowledged after 3 retries!
Error: Parition 0xbb not found in TSV File
Error: TSV flashing service failed
I already read the documentation and says that i can not able to change the mappping of the partitions only i can update de content or delete it , but this is not the case because i am not able to burn the default image form the manufactured.
Why is this problem?
How i can to change the eMMC mapping?
How i change the mapping of the partitions without using the SD?
iThank you, i have various days and not progress