Install OpenSTLinux sources offline computer
Good morning,
I am trying to setup STM32CubeIDE to work on an offline computer, I do not have the option to connect it to the internet.
Installing the SDK through the IDE works fine and I am able to import the OpenSTLinux source projects (Linux, U-Boot, TF-A/SP-Min and Op-TEE). but this is not what I need.
What I really need is to have the same result in an offline environment, this is what I do:
1) Install OpenSTLinux SDK via script as explained in the Developer Package instructions.
2) Install STM32CubeIDE 1.8.0/1.9.0
3) Configure STM32CubeIDE Preferences menu for "STM32Cube->OpenSTLinux SDK Manager" to point to my SDK installed in step 1
4) Install FW Package for stm32mp1
From this point I am able to create projects and compile for stm32mp1
But I am not able to import the OpenSTLinux Source projects
I am working with the stm32mp1 MPU (stm32mp157f-ev1 board) and I tried using STMCubeIDE 1.8.0 and 1.9.0 versions with the same results.
How can I install offline the SDK so the STM32CubeIDE is able to import the mentioned projects?
PS: I noticed that when installing the SDK though the IDE (online mode) the eclipse is installing 2 plugins. OpenSTLinux SDK openstlinux and OpenSTLinux Sources, does this have anything to do with the issue? Where can I download these plugins from to install them offline?
Thank you,
Andrés