IPCC interrupt issue in stm32mp157A ?
Hello,
We are using STM32MP157A.
We are working on IPCC from A7-0,A7-1 to M4.
We are getting IPCC interrupt A7-1 to M4,But when we are not getting interrupt from A7-0 to M4.
In cubeMx it is showing NVIC to IPCC RX1 and TX1, but not showing to RX0,TX0.
we are using CubeMX 6.3.0 and firmware version is STM32Cube_FW_MP1_V1.4.0.
But in reference manual showing IPCC_RX0,IPCC_TX0 these interrupts are available.
in our application we need interrupts both A7_0 ,A7_1 processors to M4 controller.
please help us in this regards.
regards
srikanth