Programming on board eMMC using Cube Programmer
Hi,
We have a custom board with onboard eMMC which is connected on SDMMC2 lines:
SDMMC2_D0 - PB14
SDMMC2_D1 - PB15
SDMMC2_D2 - PB3
SDMMC2_D3 - PB4
SDMMC2_D4 - PB8
SDMMC2_D5 - PB9
SDMMC2_D6 - PC6
SDMMC2_D7 - PC7
SDMMC2_CMD - PG6
SDMMC2_CLK - PE3
These pins are not all default pins for SDMMC2 so I'm interested if there is a way to program this eMMC using DFU mode with Cube Programmer. Is there a way to change pins which are used for programming?
Best regards,
Nenad