Regression with CubeIDE V1.2.0 - Breakpoint ignored ?
Hi everybody,
I've just installed STM32CubeIDE 1.2.0 on Ubuntu 18.04.
It seems that breakpoints on Cortex-M4 don't work.
When I debug via ST-Link on stm32mp157c-dk2 everything is fine but breakpoints, they are simply ignored.
Any suggestion?
With previous installation (STM32CubeIDE 1.1.0) breakpoints on Cortex-M4 worked well, allowing to stop execution wherever I wanted.
In the "Progress" tab in Eclipse it seems that Configuring GDB hangs on (at 93%), even if the execution really starts.