STM32 MP157 SSH Debugging
- September 12, 2023
- 3 replies
- 3581 views
Hello, I currently working with a STM32MP157D-DK1 Development Board. I populated the board with a prebuild openstlinux 6.1 build. A SSH connection via console is successful.
To get the M4 microcontroller running I was able to build a .elf file from the GPIO_EXTI example given by the STM32Cube_FW_MP1_V1.6.0. The .elf can be uploaded into the /boot/ directory via the scp command. By configuring Boot From an SD Card the M4 starts running an executes the just uploaded .elf file.
In order to debug the software I want to use the STM32CubeIDE Debug Configuration 'thru Linux core (Production mode)'. Unfortunatly I'm not able to connect my board with the given Target status widget, which is necessary for a successful connection build up. When i try to connect my board via the "Connections" Window -> right click SSH setup -> "Open Connection", I get the following generic error:
"
Error opening connections
Session.connect: java.net.ConnectException: Connection timed out: connect
"
Creating a connection by clicking "Open Command Shell" works aswell. Trying to Debug and Flash via the ST-Link USB Connection works without any problems. Has anyone an idea where the problem is hidden?
Firmware:
- stm32mp1-openstlinux-6.1-yocto-mickledore-mp1-v23.06.21
Programm Switch:
- 1 = ON
- 2 = ON
STM32CubeIDE
- Version: 1.13.1
- Build: 17479_20230728_0839 (UTC)
Setup
- Ethernet Cable connected (SSH via Console approved)
- Power Supply enabled
SSH Config Propertys:
- Host : 192.168.2.99
- User: root
- Public Key based authentication: enabled