STM32CubeIDE M4 debugging timed out on custom image.
I have a custom built buildroot image on my STM32MP157C-DK2. Used STM32CubeIDE 1.5.0 to create a M4 blinky project. Can download and run the .elf manually on the board, LED blinks okay. Engineering Mode works too. In Production Mode, I can download the .elf from IDE. Have to enter my credentials and see the download progress and the resulting .elf on the board.
But, after download, I have to enter the same credentials again and .. finally get:
Error in final launch sequence:
Failed to execute MI command:
target remote 192.168.2.44:3333
Error message from debugger back end:
192.168.2.44:3333: Connection timed out.
Failed to execute MI command:
target remote 192.168.2.44:3333
Error message from debugger back end:
192.168.2.44:3333: Connection timed out.
192.168.2.44:3333: Connection timed out.There serial connection says:
[ 2174.385112] remoteproc remoteproc0: stopped remote processor m4
[ 2179.484162] remoteproc remoteproc0: powering up m4
[ 2179.493251] remoteproc remoteproc0: Booting fw image Hello_stm32mp157c_dk2_CM4.elf, size 2489804
[ 2179.500701] remoteproc remoteproc0: header-less resource table
[ 2179.506452] remoteproc remoteproc0: no resource table found for this firmware
[ 2179.513765] remoteproc remoteproc0: header-less resource table
[ 2179.519465] remoteproc remoteproc0: remote processor m4 is now up
-ne
-sh: -ne: not foundDon't get, what's missing. There is a local gdbserver in the image. Is there an option to increase verbosity, i.e. to find out what the credentials are needed for 2nd time etc..?
Thanks
KnarfB