STM32CubeMX how to change OpenAMP settings
Hello,
A question on STM32CubeMX v6.16.1, when I select OpenAMP in Middleware and Software Packs, I can see configuration options, like COMMUNICATION_MODE, SHM_START_ADDRESS, SHM_SIZE etc, but they are all greyed out and not allowing me to change anything.
Is there a way to change these options in STM32CubeMX GUI? (I'm aware that the code generated by CubeMX is cutrrently broken so CubeIDE cannot build this code, and I hope for the fix in the next CubeMX version).
Another question - the code in CM33/ folder that is generated by CubeMX, can it be built by the Yocto bitbake, like it does for CA35/ folder?
Thanks!
Regards,
Sergei