Skip to main content
Associate III
January 17, 2024
Solved

STM32MP13 empty STM32Cube project "hello world"

  • January 17, 2024
  • 2 replies
  • 2633 views

Hello

Can I use Windows and STM32CubeIDE to develop application using STM32MP135FAF7 (STM32MP135F-DK discovery kit).

I tried to create empty project based on this discovery kit but it ended with message

"This project requires OpenSTLinux version 'openstlinux-6.1.-yocto-mickledore-mp1-v23.06.21', setup it now ?"

and finally error message "This operation is only supported on Linux!"

I would like to program "bare" A7 chip using STM32IDE using STLink, is it really possible ?

Thanks in advance... and Best Regards

Radim

Best answer by Erwan SZYMANSKI

@ravo ,
Some attention point that could help your case :
1) Did you double check that connectivity was good (cf the article) and the boot pins are set to "engineering mode" ? 
2) Did you double check your Debug Configuration regarding following article ? https://wiki.st.com/stm32mpu/wiki/STM32CubeMP13_Package_-_Getting_started#Download_and_run_an_example_from_SYSRAM

Kind regards,
Erwan.

2 replies

Erwan SZYMANSKI
Technical Moderator
January 17, 2024

Hello @ravo ,
Can you explain the process you followed to create your project ?
Are you sure you are using the right CubeIDE / CubeMX version mentioned in the wiki ? Please take care to follow this article and come back to me if you still face any trouble : https://wiki.st.com/stm32mpu/wiki/STM32CubeMP13_Package_-_Getting_started

Kind regards,
Erwan.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
ravoAuthor
Associate III
January 17, 2024

Dear @Erwan SZYMANSKI,

thanks for response. I fellow up already steps from AN5360 (an5360-getting-started-with-projects-based-on-the-stm32mp1-series-in-stm32cubeide-stmicroelectronics.pdf)

STM32 New Project

Board Selector - STM32MP135F-DK

I forgot to swap to bareMetal. I must have been blind

ravo_0-1705503327985.png

In meanwhile I also tried another approach to generate IOC with CubeMX and import to CubeIDE it will create working project... I was still wondering where I made a mistake in CubeIDE.

So many thanks for these another wiki pages.

So project creation works fine now. No I can compile it, but how to program/ debug project ?

When I tried to run/debug it will halt:

 

Open On-Chip Debugger 0.12.0-00024-gc3ff39f8b (2023-06-26-16:51) [https://github.com/STMicroelectronics/OpenOCD]

Licensed under GNU GPL v2

For bug reports, read

http://openocd.org/doc/doxygen/bugs.html

srst_only srst_pulls_trst srst_gates_jtag srst_open_drain connect_deassert_srst

Info : Listening on port 6666 for tcl connections

Info : Listening on port 4444 for telnet connections

Info : STLINK V3J13M4B5S1 (API v3) VID:PID 0483:3753

Info : Target voltage: 3.303605

Info : Unable to match requested speed 5000 kHz, using 3300 kHz

Info : Unable to match requested speed 5000 kHz, using 3300 kHz

Info : clock speed 3300 kHz

Info : stlink_dap_op_connect(connect)

Info : SWD DPIDR 0x6ba02477

Info : stlink_dap_op_connect(connect)

Info : SWD DPIDR 0x6ba02477

Info : STM32MP135FAFx.cpu: hardware has 6 breakpoints, 4 watchpoints

Info : gdb port disabled

Info : gdb port disabled

Info : starting gdb server for STM32MP135FAFx.cpu on 3333

Error: couldn't bind gdb to socket on port 3333: No error

shutdown command invoked

I have upgraded STLink on discovery board and it is recognised in Windows devices. But don't know where could be another problem.

Best regards

Radim

 

Erwan SZYMANSKI
Erwan SZYMANSKIBest answer
Technical Moderator
January 17, 2024

@ravo ,
Some attention point that could help your case :
1) Did you double check that connectivity was good (cf the article) and the boot pins are set to "engineering mode" ? 
2) Did you double check your Debug Configuration regarding following article ? https://wiki.st.com/stm32mpu/wiki/STM32CubeMP13_Package_-_Getting_started#Download_and_run_an_example_from_SYSRAM

Kind regards,
Erwan.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
ravoAuthor
Associate III
January 19, 2024

Dear @Erwan SZYMANSKI 

Update:

After restarting PC the gdb server now seems start working. I am now able to start debugger and run code...

Regards

Radim

Erwan SZYMANSKI
Technical Moderator
January 19, 2024

Hello @ravo ,
Thank you for your feedback. I am glad to hear it.

Kind regards,

Erwan.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.