Skip to main content
Nuzie
Associate
October 7, 2019
Question

STM32MP157 discovery board SD card population using STM32CubeProgrammer fails

  • October 7, 2019
  • 7 replies
  • 3538 views

Why does it fail reading the file, which seems to be the biggest one also ?

Log:

12:20:36 : STM32CubeProgrammer API v2.1.0

12:20:38 : USB speed : High Speed (480MBit/s)

12:20:38 : Manuf. ID : STMicroelectronics

12:20:38 : Product ID : DFU in HS Mode @Device ID /0x500, @Revision ID /0x0000

12:20:38 : SN : 004200203338510534383330

12:20:38 : FW version : 0x0110

12:20:38 : Device ID : 0x0500

12:20:46 : Read TSV File: C:\stm32mp1-openstlinux-4.19-thud-mp1-19-02-20\images\stm32mp1\flashlayout_st-image-weston\FlashLayout_sdcard_stm32mp157c-dk2-trusted.tsv

12:20:46 : Number of partitions: 9

12:21:08 : Start Embedded Flashing service

12:21:08 : Error: The file activePartitions.tsv does not exist, please check the file's path

12:21:08 : Error: TSV flashing service failed

12:21:14 : Start Embedded Flashing service

12:21:14 : Error: The file activePartitions.tsv does not exist, please check the file's path

12:21:14 : Error: TSV flashing service failed

12:21:19 : Start Embedded Flashing service

12:21:19 : Error: The file activePartitions.tsv does not exist, please check the file's path

12:21:19 : Error: TSV flashing service failed

12:21:23 : Start Embedded Flashing service

12:21:23 : Error: The file activePartitions.tsv does not exist, please check the file's path

12:21:23 : Error: TSV flashing service failed

12:21:27 : Start Embedded Flashing service

12:21:27 : Error: The file activePartitions.tsv does not exist, please check the file's path

12:21:27 : Error: TSV flashing service failed

12:21:30 : Start Embedded Flashing service

12:21:30 : Memory Programming ...

12:21:30 : Opening and parsing file: tf-a-stm32mp157c-dk2-trusted.stm32

12:21:30 : File : tf-a-stm32mp157c-dk2-trusted.stm32

12:21:30 : Size : 245360 Bytes

12:21:30 : Partition ID : 0x01 

12:21:30 : Download in Progress:

12:21:31 : File download complete

12:21:31 : Time elapsed during download operation: 00:00:00.796

12:21:31 : RUNNING Program ... 

12:21:31 : PartID: :0x01 

12:21:31 : Start operation done successfully at partition 0x01

12:21:31 : Flashlayout Programming ...

12:21:31 : Running Flashlayout Partition ...

12:21:31 : Flashlayout partition started successfully

12:21:31 : Memory Programming ...

12:21:31 : Opening and parsing file: u-boot-stm32mp157c-dk2-trusted.stm32

12:21:31 : File : u-boot-stm32mp157c-dk2-trusted.stm32

12:21:31 : Size : 748660 Bytes

12:21:31 : Partition ID : 0x03 

12:21:31 : Download in Progress:

12:21:33 : File download complete

12:21:33 : Time elapsed during download operation: 00:00:01.539

12:21:33 : RUNNING Program ... 

12:21:33 : PartID: :0x03 

12:21:33 : reconnecting the device ...

12:21:40 : USB speed : High Speed (480MBit/s)

12:21:40 : Manuf. ID : STMicroelectronics

12:21:40 : Product ID : USB download gadget@Device ID /0x500, @Revision ID /0x0000

12:21:40 : SN : 004200203338510534383330

12:21:40 : FW version : 0x0110

12:21:40 : Device ID : 0x0500

12:21:40 : Start operation done successfully at partition 0x03

12:21:40 : Memory Programming ...

12:21:40 : Opening and parsing file: tf-a-stm32mp157c-dk2-trusted.stm32

12:21:40 : File : tf-a-stm32mp157c-dk2-trusted.stm32

12:21:40 : Size : 245360 Bytes

12:21:40 : Partition ID : 0x04 

12:21:40 : Download in Progress:

12:21:40 : File download complete

12:21:40 : Time elapsed during download operation: 00:00:00.458

12:21:40 : RUNNING Program ... 

12:21:40 : PartID: :0x04 

12:21:40 : Start operation done successfully at partition 0x04

12:21:40 : Memory Programming ...

12:21:40 : Opening and parsing file: tf-a-stm32mp157c-dk2-trusted.stm32

12:21:40 : File : tf-a-stm32mp157c-dk2-trusted.stm32

12:21:40 : Size : 245360 Bytes

12:21:40 : Partition ID : 0x05 

12:21:40 : Download in Progress:

12:21:41 : File download complete

12:21:41 : Time elapsed during download operation: 00:00:00.615

12:21:41 : RUNNING Program ... 

12:21:41 : PartID: :0x05 

12:21:41 : Start operation done successfully at partition 0x05

12:21:41 : Memory Programming ...

12:21:41 : Opening and parsing file: u-boot-stm32mp157c-dk2-trusted.stm32

12:21:41 : File : u-boot-stm32mp157c-dk2-trusted.stm32

12:21:41 : Size : 748660 Bytes

12:21:41 : Partition ID : 0x06 

12:21:41 : Download in Progress:

12:21:42 : File download complete

12:21:42 : Time elapsed during download operation: 00:00:01.318

12:21:42 : RUNNING Program ... 

12:21:42 : PartID: :0x06 

12:21:42 : Start operation done successfully at partition 0x06

12:21:42 : Memory Programming ...

12:21:42 : Opening and parsing file: st-image-bootfs-openstlinux-weston-stm32mp1.ext4

12:21:42 : File : st-image-bootfs-openstlinux-weston-stm32mp1.ext4

12:21:42 : Size : 64 MBytes

12:21:42 : Partition ID : 0x21 

12:21:42 : Download in Progress:

12:23:45 : File download complete

12:23:45 : Time elapsed during download operation: 00:02:02.581

12:23:45 : RUNNING Program ... 

12:23:45 : PartID: :0x21 

12:23:45 : Start operation done successfully at partition 0x21

12:23:45 : Memory Programming ...

12:23:45 : Opening and parsing file: st-image-vendorfs-openstlinux-weston-stm32mp1.ext4

12:23:45 : File : st-image-vendorfs-openstlinux-weston-stm32mp1.ext4

12:23:45 : Size : 16 MBytes

12:23:45 : Partition ID : 0x22 

12:23:45 : Download in Progress:

12:24:16 : File download complete

12:24:16 : Time elapsed during download operation: 00:00:30.836

12:24:16 : RUNNING Program ... 

12:24:16 : PartID: :0x22 

12:24:16 : Start operation done successfully at partition 0x22

12:24:16 : Memory Programming ...

12:24:16 : Opening and parsing file: st-image-weston-openstlinux-weston-stm32mp1.ext4

12:24:16 : Error: Error while reading the file

12:24:16 : Error: Download partition 0x23 failed

12:24:16 : Error: TSV flashing service failed

14:33:53 : Start Embedded Flashing service

14:33:53 : Memory Programming ...

14:33:53 : Opening and parsing file: st-image-weston-openstlinux-weston-stm32mp1.ext4

14:33:53 : Error: Error while reading the file

14:33:53 : Error: Download partition 0x23 failed

14:33:53 : Error: TSV flashing service failed

This topic has been closed for replies.

7 replies

PatrickF
Technical Moderator
October 9, 2019

Hello,

Might be linked to PC filesystem issue (file protection, file already open, too slow system, etc..), could you please add details on your PC setup (including if windows, Linux, Virtual Machine, etc...) ?

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.NEW ! Sidekick STM32 AI agent, see here
Nuzie
NuzieAuthor
Associate
October 9, 2019
Hi Thanks for replying, As the log says, the PartID 0x23 fails, The rest of the files do succeed to populate. Please look at the end of the log, the starting of the log may contain older log lines, which are not part of the process in test. My pc runs windows 10 64 bit, 16G ram I7 core 7600u thanks Sent from Mail<> for Windows 10
PatrickF
Technical Moderator
October 10, 2019

That's sound strange, many people use that way without any issues.

Some clues below (you may already done it):

Did you use command line or CubeProgrammer GUI ? Command line under W10 should look like :

"%ProgramFiles%\STMicroelectronics\STM32Cube\STM32CubeProgrammer\bin\STM32_Programmer_CLI.exe" -c port=usb1 -w flashlayout_st-image-weston\FlashLayout_sdcard_stm32mp157c-dk2-trusted.tsv

Did you use the binaries as delivered or recompiled ?

Could you try re-populating the st-image-weston-openstlinux-weston-stm32mp1.ext4 file ?

Did you try rebooting your machine, the file might be locked by a previous attempt or another process ?

Could you try running CubeProgrammer as Administrator ?

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.NEW ! Sidekick STM32 AI agent, see here
TJann.1
Associate
March 24, 2020

Hello,

Got the same trouble with STM32CubeProgrammer V2.4.0 running Under Windows 10 64. see attached log.

the problem is on the file "st-image-weston-openstlinux-weston-stm32mp1.ext4"

I tried to:

reboot

run as administrator

the command line did not work.

Can you help me ?

Nuzie
NuzieAuthor
Associate
March 24, 2020

Hi, Sorry, i did not find a solution to it. i just populated my SD card under linux shell with a script provided by ST

TJann.1
Associate
March 24, 2020

Hi,

thanks for reply Nuzie.

Finally It works using the command line interface with STM32_Programmer_CLI.exe. I have to copy the "STM32MP15-Ecosystem-v1.2.0\Starter-Package\stm32mp1-openstlinux-20-02-19\images\stm32mp1" folder to the "C:\Program Files (x86)\STMicroelectronics\STM32Cube\STM32CubeProgrammer\bin" in order to find the files.

I hope ST will find a solution in the future for using the GUI interface.

Best regards.

TJann.1
Associate
March 24, 2020

See attached the PowerShell screen of the STM32_Programmer_CLI.exe version.

TLI.11
ST Employee
August 6, 2020

Dear ALL:

This issue is solved by update STM32-CubeProgrammers to the latest version V2.5.

So, you only need upgrade software version now.

https://www.st.com/content/st_com/en/products/development-tools/software-development-tools/stm32-software-development-tools/stm32-programmers/stm32cubeprog.html#get-software

BSchi.1
Visitor II
September 27, 2020

Hello,

i have the same problem with the STMCupeProgramme v2.5.0 too.

12:40:07 : Error: Unable to open the file st-image-bootfs-openstlinux-weston-stm32mp1.ext4

12:40:07 : Error: Download partition 0x21 failed

Therefore it seems it could be a other problem.

PatrickF
Technical Moderator
September 29, 2020

Using CubeProgrammer GUI, did you set correctly the field 'Binaries Path' ? By default it point to same folder than .tsv. For Started package, binaries are two levels up than .tsv.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.NEW ! Sidekick STM32 AI agent, see here