STM32MP157 ECO 6.0.0 Kernel custom device tree compilation fails
Executed from the linux tree root where the kernel was build from
The dts was placed in the arch/arm/boot/dts/st/ folder. {STM32MP_PROJECT} is the filename (and hardcoding the dt filename gives the same result)
Followed the wiki and the kernel HOWTO readme (both have different instructions)
https://wiki.st.com/stm32mpu/wiki/How_to_compile_the_device_tree_with_the_Developer_Package
make V=1 ARCH=arm st/stm32mp157a-dk1.dtb LOADADDR=0xC2000040 O="${OUTPUT_BUILD_DIR}"
OK
make V=1 ARCH=arm st/${STM32MP_PROJECT}.dtb LOADADDR=0xC2000040 O="${OUTPUT_BUILD_DIR}"
FAILS
make ${IMAGE_KERNEL} O="${OUTPUT_BUILD_DIR}" KBUILD_EXTDTS="${EXTDT_DIR}/linux" ${STM32MP_PROJECT}.dtb
FAILS
The error reported is No rule to make ... etc..
Since ECO 6.0 boards are now in subfolders under configs. ST's dt's in the same folder compile fine. The file is there with the correct name. Make/Makefile seems to execute some kind of scripts which i can't follow. Perhaps custom DT's not in the Makefile were never tested/considered ? P.S Why is there a LOADADDR needed for this ?