TF-A Exception on boot-up
I have a custom board built upon the stm32mp157f. (Therefore, have custom device trees.)
I currently am seeing an exception in TF-A that I cannot explain.
INFO: Reset reason (0x14):
INFO: Pad Reset from NRST
INFO: PMIC version = 0x21
INFO: FCONF: Reading TB_FW firmware configuration file from: 0x2ffe3000
INFO: FCONF: Reading firmware configuration information for: stm32mp_io
INFO: Using EMMC
INFO: Instance 2
INFO: Boot used partition fsbl1
NOTICE: BL2: v2.4-r1.0(debug):v2.4-dirty
NOTICE: BL2: Built : 16:43:51, Nov 17 2020
INFO: BL2: Doing platform setup
INFO: RAM: DDR3-DDR3L 16bits 533000Khz
WARNING: Couldn't find property st,phy-cal in dtb
INFO: Memory size = 0x20000000 (512 MB)
ASSERT: drivers/partition/gpt.c:24After the initial flashing of the eMMC with the STMCubeProgrammer, it boots fine the first time. Every boot thereafter (cold or warm), I get the above exception.
Any idea what this means, how to debug or solve it?