Trying to compile a simple helloworld.cpp on the STM32M157C discovery kit
I am trying to cross compile a simple helloworld.cpp program.
#include <iostream>
int main(int argc, char** argv)
{
std::cout << "Hello World" << std::endl;
return 0;
}
The makefile is
PROG = helloworld
SRCS = helloworld.cpp
CLEANFILES = $(PROG)
# Add / change option in CFLAGS and LDFLAGS
CFLAGS += -Wall $(shell pkg-config --cflags gtk+-3.0)
LDFLAGS += $(shell pkg-config --libs gtk+-3.0)
all: $(PROG)
$(PROG): $(SRCS)
$(CC) -o $@ $^ $(CFLAGS) $(LDFLAGS)
clean:
rm -f $(CLEANFILES) $(patsubst %.c,%.o, $(SRCS))
I have the developer package installed and I am able to compile the gtk_hello_world.c example just fine but If I try the above code it complies just fine but during the link it complains about std::cout and std::endl amoung other things related to iostream.
/home/lharris/STM32CubeIDE/Developer-Package/SDK/sysroots/x86_64-ostl_sdk-linux/usr/libexec/arm-ostl-linux-gnueabi/gcc/arm-ostl-linux-gnueabi/12.3.0/ld: /tmp/ccoeJuW6.o: in function `main':
/home/lharris/Projects/HelloWorld1/helloworld.cpp:5: undefined reference to `std::cout'
and so on...
How can I compile a simple command line program using c++ conventions or is the needed library not in the cross development tool chain?