tsv files are not uploaded to emmc due to fsbl. How to create a new fsbl file? (not STM32MP157C-EV1)
Hello, I ask for your help.
My problem is I have my own custom board, I don't know how to make fsbl binary.
I have a evaluation board, STM32MP157C-EV1.
I did a Distribution package by Yocto System.
The FlashLayout_emmc_stm32mp157c-ev1-optee.tsv file was created and I uploaded it to EMMC.
Of course, I used that program 'STM32CubeProgrammer'.
Here is the link I referenced:
https://wiki.st.com/stm32mpu/index.php/STM32MP1_Distribution_Package
Here is the manifestation I used:
DISTRO=openstlinux-eglfs MACHINE=stm32mp1 source layers/meta-st/scripts/envsetup.sh
bitbake st-example-image-qt
The result is successful, STM32MP157C-EV1.
But, The problem is custom board. AP is the same. STM32MP157AAA3.
TSV Files using the STM32CubeProgrammer program cannot be uploaded to custom board.
custom board's device tree created by CubeMX. But the problem is fsbl.
I need to build a new fsbl binary file. However, I don't know how to build it.
I don't know where the manual or method is. Please help me with this.
#Opt Id Name Type IP Offset Binary
- 0x01 fsbl1-boot Binary none 0x0 tf-a-stm32mp157c-ev1-trusted.stm32
- 0x03 ssbl-boot Binary none 0x0 u-boot-stm32mp157c-ev1-optee.stm32
P 0x04 fsbl1 Binary mmc1 boot1 tf-a-stm32mp157c-ev1-optee.stm32
P 0x05 fsbl2 Binary mmc1 boot2 tf-a-stm32mp157c-ev1-optee.stm32
P 0x06 ssbl Binary mmc1 0x00080000 u-boot-stm32mp157c-ev1-optee.stm32
P 0x0A teeh Binary mmc1 0x00280000 tee-header_v2-stm32mp157c-ev1-optee.stm32
P 0x0B teed Binary mmc1 0x00300000 tee-pageable_v2-stm32mp157c-ev1-optee.stm32
P 0x0C teex Binary mmc1 0x00380000 tee-pager_v2-stm32mp157c-ev1-optee.stm32
P 0x21 bootfs System mmc1 0x00400000 st-image-bootfs-openstlinux-eglfs-stm32mp1.ext4
P 0x22 vendorfs FileSystem mmc1 0x04400000 st-image-vendorfs-openstlinux-eglfs-stm32mp1.ext4
P 0x23 rootfs FileSystem mmc1 0x05400000 st-example-image-qt-openstlinux-eglfs-stm32mp1.ext4
P 0x24 userfs FileSystem mmc1 0xC5400000 st-image-userfs-openstlinux-eglfs-stm32mp1.ext4
To summarize, tsv files are not uploaded to emmc due to fsbl.